Drive_Working_Settings

Index.Sub 2200.2H
Data Type Unsigned16
Access Read/Write
PDO Mappable RX_PDO (1)
Unit --

Range

0 to FFFFH
Default Value --
Store Supported Yes
Description

This object is used to parametrize drive working modalities.

Bit #

Name

Description

Default Value

0

Forward_Limit_Switch_Check

1 = Forward limit switch check enabled

0 = Forward limit switch check disabled

0

1

Backward_Limit_Switch_Check

1 = Backward limit switch check enabled

0 = Backward limit switch check disabled

0

2

Fast_Stop_From_Input  (1)

1 = Fast Stop Input enabled

0 = Fast Stop Input disabled

0

3

Reserved

Reserved

0

4

Feedback_Motor_Check

1 = Motor  feedback enabled (Closed Loop)

0 = Motor  feedback  disabled (Open Loop)

0

5

Reserved

Reserved

--

6

Reserved

Reserved

--

7

Disable_Digital_Outputs_FW_Handling

1 = Disable Digital_Outputs handling by firmware (All DO user free)

0 = Enable Digital_Outputs handling by firmware (Not all DO user free)

0

8

Reserved

Reserved

--

9

Reserved

Reserved

--

10

Motor_Rotation_Direction

1 = counter clockwise rotation when motor move forward

0 = clockwise rotation when motor move forward

0

11

Reserved

Reserved

--

12

Reserved

Reserved

--

13

Reserved

Reserved

0

14

Reserved

Reserved

--

15

Reserved

Reserved

--

Bit Explanation:

Forward_Limit_Switch_Check (3) :    

  • When this bit is set (1), outside of the Homing modality, the drive will check continuously for the intervention of  Forward Limit Switch (see Drive_Inputs_Setting and Drive_Inputs_Level objects). If the limit switch intervenes and the motor is running forward then the motor will stop.

  • If bit3 of DS402_Working_Settings is 0 then the Internal_limit_active bit and Fault bit of Statusword object will be set immediately and an emergency message will be send.

  • If bit3 of DS402_Working_Settings is 1 the intervention of forward limit switch is not consider a Fault.

  • When this bit is reset (0) the drive will not check for the forward limit switch at all.

Backward_Limit_Switch_Check (3) :    

  • When this bit is set (1), outside of the homing modality, the drive will check continuously for the intervention of  Backward Limit Switch (see Drive_Inputs_Setting and Drive_Inputs_Level objects). If the limit switch intervenes and the motor is running backward then the motor will stop.

  • If bit3 of DS402_Working_Settings is 0 then the Internal_limit_active bit and Fault bit of Statusword object will be set immediately and an emergency message will be send.

  • If bit3 of DS402_Working_Settings is 1 the intervention of forward limit switch is not consider a Fault.

  • When this bit is reset (0) the drive will not check for the backward limit switch at all.

Fast_Stop_From_Input (2) :    

  • When this bit is set (1) the drive will check continuously for the intervention of Fast Stop input (see Drive_Inputs_Setting and Drive_Inputs_Level objects). If the fast stop is on the state machine is kept to ‘Switch On Disabled’  until the input goes off.

  • When this bit is reset (0) the drive will not check for the fast stop input at all.

Disable_Digital_Outputs_FW_Handling:    

  • When this bit is set (1) the firmware will not set/reset automatically the digital outputs assigned to Fault and Ready/Busy functions. Whole digital outputs are available to the user.

  • When this bit is reset (0) the firmware will set/reset automatically the digital outputs assigned to Fault and Ready/Busy functions. The remaining digital outputs are available to the user.

Motor_Rotation_Direction:    

  • When this bit is set (1) the motor will rotate counter clockwise when the motion direction is forward (Position_Actual_Value object increase) and clockwise when the motion direction is backward (Position_Actual_Value object decrease).

  • When this bit is reset (0) the drive motor will rotate clockwise when the motion direction is forward (Position_Actual_Value object increase) and counter clockwise when the motion direction is backward (Position_Actual_Value object decrease).

Feedback_Motor_Check:    

  • When this bit is set (1) the drive will enable Closed Loop feature to close the motion control loop. This will optimize the motor efficiency.

  • When this bit is reset (0) the Closed Loop feature is disabled and Open Loop feature is enabled.

Notes

  • (1) available with firmware V03r05 or superior.

  • (2) available with firmware release V02r63 or superior. See Fast Stop.

  • (3) See Limit Switch Check